Click to rate and give feedback    1 2 3 4 5
How to How to 5/18/2018
Products: Automation Server, AS-B, AS-P, WorkStation, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0, 2.1

Duplicating a SmartX Server Using Restore 

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone SmartX server.

Notice

The locally stored backup set and the SmartX server need to have the same password.

Show More

To duplicate a SmartX server using restore
  1. In WorkStation, in the System Tree pane, select the server where you want to duplicate configuration data from a backup set.

  2. On the Actions menu, click Restore .

  3. In the Restore Options dialog box, in the Available restore points list, select the backup set.

  4. Select Restore configuration with new IDs checkbox to re-use the configuration data from the backup set in a new standalone SmartX server.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

Community Content

Product version

Language