Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 1/16/2019
Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 2.0, 2.1

Create Alarm Triggered Notification Wizard – Configure Alarm Triggered Notification Page

Use the Configure Alarm Triggered Notification page to create an alarm triggered notification.

Configure Alarm Triggered Notification page

Configure Alarm Triggered Notification page

Alarm Triggered Notification Page

Property

Description

Status

Select Disabled to deactivate the notification function.

Activation schedule

Enter the schedule that contains the value that activates the notification.

Schedule value when active

Enter the value, generated by the connected schedule or other multistate variable, that activates the notification.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Decimal symbo l

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Notification text

Edit the notification text.

Quick filter

Enter a word to filter on. For more information, see Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

For more information, see Alarm Substitution Codes .

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

Add condition

Click to add a condition that has to be met for the notification to be displayed or sent.

For more information, see Alarm Filters .

Remove condition

Click to remove a condition that has to be met for the notification to be displayed or sent.

For more information, see Alarm Filters .

Add row

Click to add a row to the condition.

Remove row

Click to remove the row from the condition.

Clear all

Click to clear the selected conditions.

Community Content

Product version

Language