WorkStation

413 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
1/22/2019
User Menu – Measurement System Submenu
Use the Measurement submenu to choose the measurement system for your Workstation.
1/9/2019
How Alarms Work
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
1/2/2019
Weekly Events in WorkStation
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
12/20/2018
Trend Log Lists in WorkStation
A trend log list displays all values in the trend log in a list.
12/20/2018
Showing Trend Chart Grid Lines
You show the trend chart grid lines on the x-axis and the y-axis to make the chart easier to read.
12/20/2018
Showing Markers in a Trend Log Series
You show trend log series with markers for each record to make reading easier.
12/19/2018
Editing an Event View Standard Filter
You edit a standard filter to narrow what is displayed in the Events pane or an Event View for all users in the EcoStruxure Building Operation software.
12/18/2018
Editing an Alarm View Standard Filter
You edit a standard filter to narrow what is displayed in the Alarms pane or an Alarm View for all users in the EcoStruxure Building Operation software.
12/18/2018
Editing a User Filter
You edit the user filter to temporarily display a different set of events in the Events pane or an Event View for the logged on session.
12/18/2018

Product version

Language