Device Administrator

15 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Installation Wizard – Installation Type Page
Use the Installation Type page to define which type of installation to perform when corresponding product is already installed on your computer or server.
5/18/2018
Products
Depending on your needs, you can install all Building Operation products or a few products, such a single SmartStruxure server device with a connected WorkStation.
10/31/2017
10/12/2017
Installation Overview
The Building Operation products are installed using installation packages.
12/20/2016
Installation Example
Schneider Electric recommends that you install the license server framework before other Building Operation software or SmartStruxure server devices. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.
12/14/2016
Installation Reparation
If something unexpected happens to a Building Operation product, for example, the Building Operation product does not start or software files are missing, you can try to solve the problem by repairing the installation.
12/14/2016
Reinstallation
This is an additional solution instead of first manually uninstalling the current product and then installing a new copy.
12/14/2016
Uninstallation
To uninstall a Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.
12/14/2016
Version Numbers and Parallel Installations
The Building Operation version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.
12/14/2016
System Backup
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the SmartStruxure servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.
10/13/2016

Product version

Language