AS-P

968 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
2/21/2019
Creating an Alarm Triggered Notification
You configure an alarm triggered notification to notify users when an alarm condition is met.
1/23/2019
Trend Log List Context Menu
Right-click a row in a trend log list to open the trend log list context menu, where you can edit a record, show the history of a record, or copy the trend log list data.
12/20/2018
Acknowledged Style Properties
Use the Acknowledged Style properties to edit and view the colors and fonts of alarms in Alarms pane and Alarm Views that are in acknowledged state.
12/11/2018
Communication Port Wiring
The wiring recommendations for the SmartStruxure server device communication ports apply to the wires and cables used for RS-485 communications, LonWorks communications, USB connections, and Ethernet connections. Always use the recommended cables and wires.
12/6/2018
Delete Object Dialog Box
The Delete object dialog box is displayed when you try to delete an object you are not allowed to delete.
11/12/2018
Restricting the Permission to Change the Alarm State Sort Order
You restrict the permission to change the alarm state sort order when you want to make sure that a user account group or a user account does not change the alarm state sort order for all users or alarm views in a Building Operation system.
10/2/2018
9/17/2018
Configuring Permissions to a Path
You configure the permissions users or user groups have to a path to grant or limit permissions to that path.
5/24/2018
Context-Sensitive Path Permissions
You can manage permissions by configuring the permissions for a given user account or user account group to a certain object in the System Tree pane or List View and below that object, for example, a folder and its contents.
5/24/2018

Product version

Language