Schedules

148 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Weekly Events in WorkStation
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
12/20/2018
Scrolling a Week in a Schedule
You scroll a week in a schedule using the Forward a Week and Back a Week buttons.
12/17/2018
Scrolling a Day in a Schedule
You scroll a day in a schedule using the Forward a Day and Back a Day buttons.
12/17/2018
Schedule Navigation in WorkStation
You have some navigation tools to use when you navigate the Basic Schedule Editor, the Advanced Schedule Editor, and the Calendar Editor. To navigate the editors, you can use the tools described in the following table.
12/17/2018
Priorities
Priority is a number that corresponds to a preassigned level of importance. When used in schedules, priority numbers range from one to sixteen. One is the most important or highest priority and sixteen is the lowest priority.
12/13/2018
Modifying a Schedule Using the Text View
Use the Text View of the Advanced Schedule editor to edit specific time sequences and break down a time value into hundredths of a second.
12/13/2018
Editing a Weekly Event
You edit a weekly event to change the information about a weekly event on a single day.
11/26/2018
Xenta Schedule Editor
Use the Xenta Schedule Editor to view and configure weekly events and exception events for a Xenta schedule.
11/19/2018
Modifying a Schedule Using the Graphic View
Use the Graphic View of the Advanced Schedule editor to edit the properties of an exception or weekly event.
11/16/2018
Deleting an Exception Event from a Xenta Schedule
You delete an exception event when you no longer need the exception to make an exception from a weekly event.
11/8/2018

Product version

Language