How to

722 Topic(s)
Use the filters below to limit the number of search hits.
Products
Functionality
Topic
Modified
Rating
Viewing Enterprise Server System Log
You view logged server events in the Enterprise Server system log to troubleshoot server problems that are traced to the Enterprise Server.
3/22/2017
Creating a Notification Report Template
You create a notification report template to get a notification report when an alarm or a variable triggers a notification.
3/22/2017
​Configuring Server Port Settings
You configure server HTTP, HTTPS, and TCP ports to define the communication of the different protocols. In Software Administrator, you can configure either the ports of the Enterprise Server.
3/22/2017
Repairing the Enterprise Server
​​You repair the Enterprise Server installation if any problems are caused by the current installation.
3/22/2017
Restarting the Enterprise Server Windows Service
You restart the Enterprise Server Windows service to reset or apply new settings.
3/21/2017
Duplicating an Object
You duplicate an object when you want to create several copies of an object in one single operation, for example a folder.
3/8/2017
Viewing Events in This Branch
You view events in this branch when you want to view all the events below a certain branch in the system. A branch can be any object that can contain other objects, for example, a folder or a network.
3/6/2017
Deleting a Favorite
You delete a favorite that it is no longer needed.
3/2/2017
Searching for Objects Using Simple Search
You use Simple search to search for an object by its name.
2/22/2017
Repairing WorkStation and Client Tools Installation
​You repair the WorkStation and client tools installation if any problems are caused by the current installation.
1/21/2017

Product version

Language