Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 10/12/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms, Trends
Product version: 1.9

Mass Create Object Wizard – Name Page

Use the Choosing the type and naming the object page to name the mass-created objects.

Naming the object page

Naming the object page

Naming the Object Page

Property

Description

Object type list

Select the type of object you want to mass create. For more information, see Building Operation Objects .

Prefix

Type a label that is added in front of the object name. For more information, see Suffix and Prefix .

Suffix

Type a label that is added after the object name. For more information, see Suffix and Prefix .

Description

Type a description that explains what the object is used for.

Destination

Select the destination folder option where you want to create the objects. For more information, see Mass Create Path Options .

Location

Displays the folder where the alarms or trends are created.

If you create alarms or trends in a different path, relative to each selected object, you can browse in a different location.

For more information, see Mass Create Path Options .

Community Content

Product version

Language