Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 11/6/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9

Create Alarm Wizard – Attachment Page

Use the Attachment page to add attachments to an alarm or an alarm decoration.

Attachment page

Attachment page

Attachment Page or Tab

Property

Description

Add attachment

Click to add an attachment to the alarm decoration rule. For more information, see Alarm Attachments

Remove attachment

Click to remove the selected attachment from the alarm decoration rule.

Navigate to 

Click to open the attachment that is selected in the attachment list.

Type

View the object type of the attachment.

Name

View the name of the attachment.

Display on alarm

Select to display the attachment when the alarm is triggered.

Path

View the path of the attachment.

Community Content

Product version

Language