Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 11/6/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9

Create Alarm Decoration Rule Wizard - Filter Page

Use the Filter page or tab to configure the conditions that have to be met before the alarm decoration rule overrides the original properties configured for the alarm.

Filter page

Filter page

Filter Page or Tab

Property

Description

Add condition

Click to add the conditions that have to be met before the alarm decoration rule becomes active and overrides the original configuration of the alarm. For more information, see Add/Remove Conditions Dialog Box .

Remove condition

Click to remove the selected condition.

Add row

Click to add another condition that has to be met before the alarm decoration rule becomes active.

Remove row

Click to remove the selected alarm decoration rule condition.

Clear all

Click to clear the selected conditions.

Community Content

Product version

Language