Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 12/29/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: User Management
Product version: 1.9

User Account Properties

Use the User Account properties dialog box to configure the properties of a user account.

User account properties

User account properties

User Account Properties

Component

Description

Click to create a new user profile. For more information, see Create Object Wizard – Naming the Object Page .

Click to edit a user profile. For more information, see Profile Properties .

Click to remove a user profile.

Disabled

Select True to disable the user account.

Force password change

Select True to force the user to change password after the initial logon.

Password

Type the password again.

Confirm Password

Type the password again.

Expires on

Enter an expiration date and time for the user account. By default, there is no expiration date for the account.

Password never expires

Select True to disable password's expiration date.

System of measurement

Displays the system of measurement for the user account.

Community Content
"Password never expires" missing benjamin.roswall@schneider-electric.com

The "Password never expires" is missing from the dialog screen shot and the text.

Click to rate and give feedback    1 2 3 4 5
Last modified: 7/27/2017

Product version

Language