Click to rate and give feedback    1 2 3 4 5
How to How to 6/26/2018
Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0

Restoring the EcoStruxure BMS Server

You restore the EcoStruxure BMS server to revert back to a previous snapshot of the EcoStruxure BMS server data.

Show More

Important Important

If your system includes the Reports Server and the Enterprise Server or Enterprise Central, stop the Reporting Agent service on the Reports Server first to prevent report generation during a restore of the Enterprise Server or Enterprise Central. For more information, see Stopping the Reporting Agent Windows Service .

To restore the EcoStruxure BMS server
  1. Stop the Reporting Agent service on the Reports Server. For more information, see Stopping the Reporting Agent Windows Service .

  2. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server that you want to restore.

  3. On the Actions menu, click Restore .

    Tip Tip

    Take manual control of any output points that could potentially damage equipment before restoring the EcoStruxure BMS server. If you cannot disconnect the physical outputs, restore the EcoStruxure BMS server using a trusted restore file that will turn off/on the outputs predictably and safely.

  4. In the Restore Options dialog box, in the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the EcoStruxure BMS server.

  5. Select the type of data you want to restore:

    • Select Configuration only to restore only configuration and custom object types' data.

    • Select All data to restore the configuration, historical, and custom object types data.

  6. Click Restore .

  7. Click Yes .

  8. Click Close .

    If your system includes the Reports Server, the Reporting Agent Windows service restarts automatically.

Community Content

Product version

Language