Click to rate and give feedback    1 2 3 4 5
Concept Concept 1/17/2018
Products: WorkStation, WebStation
Functionalities: Basic Functionality
Product version: 1.9

Modify Values

You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.

Forced Values

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

For more information, see Forced Values .

Community Content

Product version

Language