Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 6/27/2018
Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0

Backup and Restore Manager Properties (Enterprise Server) – Basic Tab

Use the Basic tab to view the current backup and restore status of an Enterprise Server. In addition, you can set the maximum number of local and remote backup sets to store so the system can purge the outdated files.

Backup and Restore Manager properties for the Enteprise Server

Backup and Restore Manager properties for the Enteprise Server

Backup and Restore Manager Properties (Enterprise Server) – Basic Tab

Component

Description

Backup folder  

Displays the storage location of the backup set.

Backup and restore status

Displays the current status, such as backing up.

Last backup 

Displays the date and time of the last successful backup.

Purge AS backup sets

Select Yes to enable automatic purging of remote SmartX server backup files at the next backup.

Purge local backup sets

Select Yes to enable automatic purging of local Enterprise Server backup files at the next backup.

Number of remote AS backup sets to store

Enter the maximum number of backup sets that the system can store for each SmartX server.

Number of local backup sets to store

Enter the maximum number of backup sets that the system can store for the Enterprise Server.

Community Content

Product version

Language