Click to rate and give feedback    1 2 3 4 5
How to How to 6/26/2018
Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0

Restoring an Enterprise Server from the Enterprise Central

You log on to an Enterprise Central to restore an Enterprise Server.

Show More

Restoring an Enterprise Server from the Enterprise Central
  1. In WorkStation, in the System Tree pane, select the Enterprise Server that you want to restore.

  2. On the Actions menu, click Restore .

  3. In the Restore Options dialog box, in the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the Enterprise Server.

  4. Select the type of data you want to restore:

    • Select Configuration only to back up only configuration and custom object types data.

    • Select All data (Configuration and Historical) to back up the configuration, historical, and custom object types data.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

Community Content

Product version

Language