Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 6/27/2018
Products: Enterprise Central, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 2.0

Backup and Restore Manager Properties (Enterprise Central) – Basic Tab

Use the Basic tab to view the current backup and restore status of an Enterprise Central. In addition, you can set the maximum number of local and remote backup sets to store so the system can purge the outdated files.

Backup and Restore Manager properties for the Enteprise Central

Backup and Restore Manager properties for the Enteprise Central

Backup and Restore Manager Properties (Enterprise Central) – Basic Tab

Component

Description

Backup folder 

Displays the storage location of the backup set.

Backup and restore status

Displays the current status, such as backing up.

Last backup  

Displays the date and time of the last successful backup.

Purge local backup sets

Select Yes to enable automatic purging of local Enterprise Central backup files at the next backup.

Number of local backup sets to store

Enter the maximum number of backup sets that the system can store for the Enterprise Central.

Community Content

Product version

Language