Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 12/5/2017
Products: Automation Server, Enterprise Server, AS-P
Functionalities: I/NET
Product version: 1.9

DCU Device Properties – Message Distribution Tab

Use the Message Distribution tab to view and configure message distribution settings and reliable tap settings on the selected I/NET DCU.

DCU device properties - Message Distribution tab

DCU device properties - Message Distribution tab

DCU Device Properties - Message Distribution Tab

Component

Description

Distribution group

Select a distribution group that matches a host workstation distribution group in order to ensure the message masks are matched. For a message mask to match, it must be part of the correct distribution group.

Distribution mask

Activate the mask position(s) corresponding to the workstation(s) that should receive messages originating from this device. Both the distribution group and at least one active mask position must match to receive messages.

Message priority

Select the priority for messages originating from this device.

Reliable tap

Select a non-zero value to enable reliable messaging. The value you select represents the station address of the tap (or device emulating a tap) that is being used to route messages from this controller to an I/NET host.

Community Content

Product version

Language