Click to rate and give feedback    1 2 3 4 5
Concept Concept 8/9/2018
Products: MP-C, MP-V
Functionalities: Hardware
Product version: 2.0

MP Series Controller LEDs

There are five LEDs on the front panel of the MP Series controller.

MP Series controller LEDs

MP Series controller LEDs

MP Series Controller LEDs

Function

Color

Status (MP Series controller)

Green/Red

Sensor Bus Tx

Yellow

Sensor Bus Rx

Green

Ethernet 1

Green/Yellow

Ethernet 2

Green/Yellow

Note Note

The MP Series controller Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the MP Series controller and the ongoing communication.

Status LED

The MP Series controller Status LED indicates the condition of the device.

MP Series Controller Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

MP Series controller application running

Green, flashing (~1 Hz)

Device restarting, wait

MP Series controller application running

Red, constant

Fatal error - attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

MP Series controller I/O board receiving software upgrade, wait

Amber, constant

MP Series controller boot applet running

Amber, flash

Device restarting, wait

MP Series controller boot applet started

Sensor Bus LEDs

The Sensor Bus LEDs indicate the condition of the sensor bus data communication.

Sensor Bus LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LEDs

The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication.

Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

Green/yellow, constant

10/100 Mbit link connected, no activity

No light

No link, no activity

Community Content

Product version

Language