Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 8/3/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Functionalities: Alarms, Basic Functionality, Engineering, Import/Export, Schedules, Trends
Product version: 1.9

List View Context Menu

Use the List View context menu to perform a number of operations on the selected object or objects.

List View context menu

List View context menu

List View Context Menu

Command

Description

New

Click to open the New submenu where you add new objects.

Import

Click to import an object to the Building Operation system.

Advanced

Click to open the Advanced submenu where you select or clear content types or find out which objects that are using the selected content type. For more information, see List View Context Menu - Advanced Submenu .

Cut

Click to cut the selected object.

Copy

Click to copy the selected object.

Paste

Click to paste a cut or copied object.

Paste as shortcut

Click to paste the path to an object.

Paste special

Click to paste special.

Duplicate

Click to duplicate the selected object.

Move

Click to select a different location for the selected object.

Delete

Click to delete the selected objects.

Rename

Click to rename the selected object.

Create shortcut

Click to create a shortcut to the selected object.

List View settings

Click to open the List View settings submenu. For more information, see List View Context Menu - List View Settings Submenu .

Community Content

Product version

Language