Click to rate and give feedback    1 2 3 4 5
Concept Concept 10/12/2017
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Engineering, User Management
Product version: 1.9

Customized Navigation

You use the Navigation Pane to build a customized structure for navigation. The Navigation pane can be used in a workspace or a panel.

The content of a navigation pane is a referenced menu object. The objects in a navigation pane have the same context menus as they do in the System Tree pane. The navigation pane is static and only displays objects that were added to the menu object.

Navigation Pane components are not shown in WebStation in this version.

Community Content

Product version

Language