Click to rate and give feedback    1 2 3 4 5
How to How to 3/8/2017
Products: Automation Server, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Engineering
Product version: 1.9

Duplicating an Object

You duplicate an object when you want to create several copies of an object in one single operation, for example a folder.

Show More

To duplicate an object
  1. In WorkStation, in the System Tree pane or in the List View , select the object you want to duplicate.

  2. On the Edit menu, click Duplicate .

  3. In the Number of duplicates box, enter the number of copies you want to create.

  4. Press ENTER.

  5. In the New name column, click the name you want to change and type a new name.

  6. Click OK .

The configured number copies of are created and named according to the names in the list.

Community Content

Product version

Language