Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 1/11/2018
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9

Alarm Triggered Notification Properties - Basic Tab

Use the Basic tab to view or edit the properties of the alarm triggered notification.

Alarm triggered notification properties

Alarm triggered notification properties

Alarm Triggered Notification Properties

Property

Description

Status

Select Disabled to deactivate the notification function.

Activation schedule

Enter the schedule that contains the value that activates the notification.

Schedule value when active

Enter the value, generated by the connected schedule or other multistate variable, that activates the notification.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Notification text

Edit the notification text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

Community Content

Product version

Language