Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 1/11/2018
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 1.9

Variable Triggered Notification Properties - Basic Tab

Use the Basic tab to view or edit the properties of the variable triggered notification.

Variable triggered notification properties

Variable triggered notification properties

Variable Triggered Notification Properties

Property

Description

Trigger variable

Enter the variable that triggers the notification.

Trigger condition

Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Generate report relative to

Enter the path to the object that is relative to the generated notification report.

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Notification text

Edit the notification text.

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

Community Content

Product version

Language