Click to rate and give feedback    1 2 3 4 5
Specifications Specifications 8/2/2017
Products: Support Tools
Functionalities: Engineering
Product version: 1.8, 1.9

Automated Engineering Tool

Automated Engineering Tool

Automated Engineering Tool

Introduction

Automated Engineering Tool is a PC-based software platform that provides engineers with an efficient way to generate application content for SmartStruxure servers and Project Configuration Tool (or Project Configuration Server). Automated Engineering Tool is designed to improve the engineering quality and consistency of HVAC applications for a SmartStruxure solution while reducing the time to develop and deploy those applications.

Features

Standards and efficiency

Focused on efficiency and standardization, Automated Engineering Tool allows you to create templates based on pre-existing engineered solutions and reuse those templates on other projects or for similar applications on the same project. Automated Engineering Tool provides robust search and replace, and other functions to enable an application to be modified or renamed before deployment. Utilities provide support for transitions from legacy systems and assist in generating Building Operation objects needed for pre-commissioning.

Simplify and standardize

Automated Engineering Tool reduces the need to start from scratch by allowing a user to capture those common or standard applications and save or share them for future use. Reusing proven applications provides significant efficiency, productivity, and reliability.

Create a template

Automated Engineering Tool provides the user the ability to save any Building Operation content or application as a template. A template is self-contained database file that contains all object information, bindings, documentation, graphics, and programs in an easily transferrable format. Creating a template is simple using a familiar System Tree view just like the one found in WorkStation. You can easily select any content and save it as a new template.

Create Template

Create Template

Multiple views

You can view an application in Automated Engineering Tool using different views that provide a number of techniques to create objects and applications in a repeatable manner. Flow View, I/O View, Folder View, Graphic View, and Object View present information about the library file you are working with.

Flow View

In Flow View, I/O modules, variables, programs, and graphics are displayed in a 2-D flow diagram with the bindings that link them clearly displayed. Selecting an object highlights all of the associated bindings so you can clearly identify all the connected objects. Additional standard server objects, TGML graphics, and programs can be added and bound in this view.

Flow View

Flow View

I/O View

Use the I/O View to allocate objects to the I/O modules. The objects can be added directly in Automated Engineering Tool or uploaded from the target server. Mismatches can be identified and corrected manually or automatically.

Folder View
Folder View

Folder View

In the Folder View, the application objects can be organized into folders to match the target server. You can add new folders or rename folders. Duplicated folders and objects are clearly identified for correction. Use the Copy Wizard to quickly duplicate single folders or an entire application any number of times.

Copy Wizard

Copy Wizard

Graphic View

If a template contains a graphic file, users can see it in the Graphic View.

Object View

The Object View provides quick access to information about all the objects in your current template. You can sort and review the objects by type or name. All of the object properties are available and can easily be edited. All the bindings associated with those objects are managed and retained even as changes are made to names or properties. The Object View also provides a robust search and replace wizard.

Object View

Object View

Reuse an existing application

Automated Engineering Tool enables existing HVAC applications saved as templates to be deployed, modified, and re-used without impact on object bindings, even if objects are renamed. Solutions can be re-engineered and downloaded to a new or existing SmartStruxure server or Project Configuration Tool. Creating these HVAC applications from templates can greatly simplify your standardization efforts and help improve the consistency and repeatability of common HVAC applications.

Modify and edit

A Global Edit feature enables you to perform multiple updates on any text in the target application or template. Text can be updated or modified. Modifications can quickly be done to names, descriptions, labels, alarm text, and more. You can change text contained in Graphics, Function Block programs, and Script programs. The utility even provides a method of doing multiple find and replace using a file identifying the word pairs.

Global Edit

Global Edit

Manage bindings

As changes are made to the application, Automated Engineering Tool manages and updates the binding information. New bindings can be created in the Flow View when objects are added. In addition, you can use the Binding Manager to review the bindings for anything that is unbound. You can manage external bindings to objects only in the target SmartStruxure server. Using the Binding Manager, you can quickly manage all the additional connections required.

Binding Manager

Binding Manager

Easily and safely deploy

Automated Engineering Tool leverages the power of Workstation SDK for deploying your application. Leveraging this connection provides a simple, safe, and validated method of deploying your templates to a SmartStruxure server or Project Configuration Tool. Once connected to your target server, you can see the status as the application is deployed. Any errors or exceptions are clearly identified as the application is deployed to ensure successful transfer to Building Operation.

Deploy

Deploy

Advanced templates with configuration

For advanced users, templates can be created with additional configuration. A template can be created that contains the information for a complex application and questions can be presented that allow the user to configure the application. Based on the answers to the questions, the application and all associated objects, logic, and bindings are adjusted. These wizard templates can be combined with an Excel file to quickly duplicate the application any number of times while setting parameters specific to each one. For example, a large number of VAVs can be created and configured from one wizard template and schedule.

 Template Wizard

Template Wizard

Template Editor

To create your own wizard templates, use the Template Editor to create a series of questions that can be connected to logic that modifies the application to get to the desired state. Using a combination of variables, expressions, and tags, a complex application set up can easily be configured through a series of questions.

Template Editor

Template Editor

Design View (Swedish only)

Design View provides an additional method of configuring your applications. Libraries can be created that cover a type of application, such as an air handling unit, chiller, or fan coil unit. The user can then open the library and use drag and drop functionality to configure the application based on specific needs. Currently, the library contains only Swedish versions of applications. More libraries will follow.

Design View

Design View

Drag and drop configuration

In Design View, applications can be opened from existing templates saved on your computer. A user can open a particular library and use the Components window to drag and drop components into a TGML graphic. When the configuration is complete, you can view the TGML, review the function block programs, and compile the entire application, and deploy it to a target server.

Other time saving utilities

Automated Engineering Tool also contains some utilities to assist in engineering. Using these utilities, you can create Building Operation objects from various files. You can open those objects in Automated Engineering Tool and deploy them to a SmartStruxure server or Project Configuration Tool. The utilities provide some efficiency on certain transitions from legacy systems and when pre-commissioning a SmartStruxure server device.

Generate objects from a workbook

A workbook is an Excel file that contains information about SmartStruxure devices and the associated Input and Output. Based on input from an Excel file created from an external estimating or design tool, Automated Engineering Tool can create a template of all objects needed to deploy to the target device so that pre-commissioning can be done. Currently the UK format and the Studio 360 checkout sheets are supported.

Alarm Manager

The Alarm Manager allows a user to quickly and efficiently create new alarms. These alarms can be created from data in an Excel spreadsheet or by dragging objects from the System Tree into the Alarm Manager. You can easily view and edit your alarm data from the Alarm Manager, including the ability to do mass edits before saving the alarms to your target server.

Alarm Manager

Alarm Manager

Upgrade Utility

The Upgrade Utility facilitates some of the effort required to transition legacy systems to Building Operation. Building Operation objects can be created from text files, such as Continuum dump files (.dmp) or Satchwell Listpoint and/or Gateway files (.txt). The utility creates the Building Operation objects within a template, which then can be deployed to a SmartStruxure server device or Project Configuration Tool.

Upgrade Utility

Upgrade Utility

Supported Building Operation options

Continuum

  • I/O and Values created from Controller (*.dmp) Input, Output, and Numeric objects.

  • Modbus objects created from Controller (*.dmp) RTU, RTU Annex, and IP objects.

  • I/O mapped to BACnet objects from Controller (*.dmp) Input, Output objects.

  • b3 I/O and Values created from Controller (*.dmp) Input, Output, Numeric objects.

  • Update BACnet Alarm Message from Controller (*.dmp).

Sigma

  • Building Operation controller objects and logic converted from Sigma controller objects

  • I/O created from Outstation Listpoint (*.txt) CMD, ST, AI, AO objects.

  • I/O mapped to BACnet objects created from Outstation Listpoint (*.txt) CMD, ST, AI, AO objects.

  • Modbus objects created from Outstation Listpoint (*.txt) and gateway (*.txt) 16-bit and 32-bit.

BAS

  • I/O created from Outstation Listpoint (*.txt) CMD, ST, AI, AO objects.

  • I/O mapped to BACnet objects created from Outstation Listpoint (*.txt) CMD, ST, AI, AO objects.

  • Modbus objects created from Outstation Listpoint (*.txt) and gateway (*.txt) 16-bit.

Specifications
Server side
SmartStruxure servers
Building Operation v1.6 and later
For more information, see Enterprise Server, Automation Server, AS-P, and AS-B specification sheets.
Project Configuration Tool
Building Operation v1.8 and later
For more information, see the Project Configuration Tool specification sheet.
Project Configuration Server
Building Operation v1.6 to v1.8
Client side
Hardware requirements
Processor
Minimum: Intel Core i5 @ 2.0 GHz or equivalent
  
Recommended: Intel Core i5 @ 3.0 GHz or better
Memory
Minimum: 4 GB
  
Recommended: 8 GB or higher
Hard disk space
Minimum: 20 GB
Display
Minimum: 1,024x768 pixel resolution
Other devices
Microsoft mouse or compatible pointing device is required.
Software requirements
Operating systems
Microsoft Windows 7 (32-bit)
  
Microsoft Windows 7 (64-bit)
  
Microsoft Windows 8.1 (32-bit)
  
Microsoft Windows 8.1 (64-bit)
  
Microsoft Windows 10 (64-bit)
  
Microsoft Windows Server 2008 R2 (64-bit)
  
Microsoft Windows Server 2012 (64-bit)
  
Microsoft Windows Server 2012 R2 (64-bit)
The following Microsoft Windows 7 editions are supported: Professional, Enterprise, and Ultimate.
The following Microsoft Windows 8.1 editions are supported: Pro, Pro N, Enterprise, and Enterprise N.
The following Microsoft Windows 10 editions are supported: Pro and Enterprise.
The following Microsoft Windows Server 2008 R2 editions are supported: Standard, Web, Enterprise, Datacenter, and Itanium.
The following Microsoft Windows Server 2012 and Microsoft Windows Server 2012 R2 editions are supported: Datacenter, Standard, Essentials, and Foundation.
Required additional software
Microsoft .NET Framework 4.5 or 4.6
Community Content

Product version

Language