WorkStation

416 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Mass Rename
In WorkStation, you can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.
3/24/2017
Trend Chart Event Icons
Use the Trend Chart event icons to get information on different trend log events.
3/22/2017
How Alarms Work
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
3/15/2017
Alarm and Event Details
To quickly get all the details of a specific alarm or event in WorkStation, or an alarm in WebStation, you can use a Detail view. The Detail view always displays all properties that can be added and displayed in the Alarms pane, Events pane, Alarm View or Event View.
3/15/2017
Alarm Assignments
A triggered alarm can be manually or automatically assigned to a specific user or user group that seems to be most suited to correct the problem.
3/7/2017
Alarms Pane and Alarm View Toolbar
Use the Alarms pane and Alarm View toolbar to manage the alarms.
3/7/2017
Events Pane and Event View Toolbar
Use the Events pane and Event View toolbar to manage the events.
3/7/2017
Viewing Events in This Branch
You view events in this branch when you want to view all the events below a certain branch in the system. A branch can be any object that can contain other objects, for example, a folder or a network.
3/6/2017
Deleting a Favorite
You delete a favorite that it is no longer needed.
3/2/2017
Object-Specific Event View Toolbar
Use the Object-Specific Event View toolbar to manage how to display events.
3/1/2017

Product version

Language