WebReports

172 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
System Backup
Before upgrading the system, it is strongly recommended that you archive the historical data and back up the EcoStruxure BMS servers to preserve the current data and configurations. If you plan to upgrade WebReports, be sure to back up the Reports database in SQL Server.
6/5/2018
5/21/2018
SQL Server
Before you can install WebReports successfully, it is imperative that the SQL Server has been installed with a particular group of settings.
5/18/2018
Starting the Reporting Agent Windows Service
You start the Reporting Agent Windows service to resume collecting report data.
5/18/2018
Synchronizing WebReports with a New Report
You synchronize WebReports with a deployed report to ensure that the report displays in the WebReports Reports Tree. You use WebReports with a Web browser to complete this procedure.
5/18/2018
Top Activities Report
The Top Activities report provides information about the most frequent user and system activities for all EcoStruxure BMS servers in your system. An example of a user activity is creating or changing an object. An example of a system activity is initializing an EcoStruxure BMS server. You can enter a number to filter the top number of activities. You can then determine what activities occur most often on what EcoStruxure BMS servers, and consider ways to improve your system.
5/18/2018
Top Alarms Report
The Top Alarms report provides information about the most frequently occurring alarms for all EcoStruxure BMS servers. The EcoStruxure BMS server where the alarm originated and the monitored variable are included in the report. You can use the report to identify the number of times an alarm has been triggered and then determine the most problematic areas in your buildings. The percentage of the total number of alarms is also calculated.
5/18/2018
Top System Alarms Per Server Report
The Top System Alarms Per Server report provides information about the most frequently occurring system alarms for a particular EcoStruxure BMS server. The report can be used by System Managers to identify and troubleshoot problems with a specified EcoStruxure BMS server.
5/18/2018
Top System Alarms Report
The Top System Alarms report provides information about the most frequently occurring system alarms for all EcoStruxure BMS servers in your system. The report can be used by System Managers to identify and troubleshoot issues and problems with all EcoStruxure BMS servers.
5/18/2018
Transferring Reports Schedules
When upgrading WebReports and transferring a WebReports database from one computer to another (or to a different operating system), you also need to transfer any existing reports schedules to ensure that the schedules are available in the 64-bit computer where you want to install the next version of WebReports. Reports schedules are not stored in the WebReports database.
5/18/2018

Product version

Language