WebReports

172 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Products
Depending on your needs, you can install all Building Operation products or a few products, such a single SmartStruxure server device with a connected WorkStation.
3/29/2017
1/16/2017
12/14/2016
Creating a Meter
You create a meter within a site to represent an external meter.
12/14/2016
Creating a Site
You create a site (or a sub-site) to represent the location of a meter, or a group of meters.
12/14/2016
Creating the Energy Folder
You create the Energy folder to provide a receptacle for an energy monitoring site hierarchy.
12/14/2016
Energy Monitoring Reports
Energy monitoring reports are based on the measurement of energy at meters within a site. You need to create a hierarchy of sites and meters before you generate energy monitoring reports. The meter hierarchy provides the source from which energy reports are generated. Energy monitoring reports are contained in the Energy Monitoring folder.
12/14/2016
Engineering Tools Overview
You engineer your system using the engineering tools.
12/14/2016
Starting the Reporting Agent Windows Service
You start the Reporting Agent Windows service to resume collecting report data.
11/21/2016
Backing Up the WebReports Database
You back up the WebReports database as a precaution to ensure that you do not lose data, such as during a WebReports software upgrade.
10/13/2016

Product version

Language