WebReports

172 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Reports Icons in WorkStation
Use the Reports icons in the System Tree pane in WorkStation to open a report and to open the Report Manager.
5/18/2018
Reports Properties – Basic Tab
Use the Basic tab to view or rename the selected report.
5/18/2018
Create Report Wizard – Report Name Page
Use the Report Name page to select a report that you want to create in WorkStation.
5/18/2018
Unit Configuration Errors Report
The Unit Configuration Errors report is a WebReports Diagnostics report that enables you to identify which extended trend logs (if any) have incorrectly configured energy units. The report also contains the names of energy meters that are associated with the extended trend logs, and the system point that is logged. In addition, the Unit Configuration Errors report states whether the units are incorrectly set (that is, the wrong type of unit), or simply that no unit at all is configured.
5/18/2018
Viewing a Prompted Report in WorkStation
You view a prompted report to see a report based on filtering criteria that you enter.
5/18/2018
Viewing a Prompted Report in WebReports
You view a prompted report to see a report based on filtering criteria that you enter.
5/18/2018
Viewing a Dashboard Report in WorkStation
You view a dashboard report to see a report based on predefined filtering criteria.
5/18/2018
Viewing a Dashboard Report in WebReports
You view a dashboard report to see a report based on predefined filtering criteria.
5/18/2018
Starting a Windows Service
You start a Windows service in Windows after an installation, upgrade, or update.
5/18/2018
Deleting an Energy Object Tag
You delete an energy object tag to remove it from the Tags folder when the tag is no longer required.
5/18/2018

Product version

Language