Enterprise Server

940 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Products
Depending on your needs, you can install all Building Operation products or a few products, such a single SmartStruxure server device with a connected WorkStation.
3/29/2017
Object Properties
Every object in Building Operation has a number of different properties. Properties can be of two different types: read only and read/write. Read only properties are dimmed and cannot be changed. Read/write properties can be changed.
3/25/2017
Mass Rename
In WorkStation, you can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.
3/24/2017
Viewing Enterprise Server System Log
You view logged server events in the Enterprise Server system log to troubleshoot server problems that are traced to the Enterprise Server.
3/22/2017
Server Installation Wizard – Configuration Page
Use the Configuration page to configure the port number the Enterprise Server listens to when communicating through a specific protocol.
3/22/2017
Licenses
Building Operation uses two types of licenses: the network license and the local license. Network licenses are the most common type of license in Building Operation. With network licenses, only the number of licenses that are used at the same time are required. The local license is often time limited and used to test and run a system that is under construction.
3/22/2017
Creating a Notification Report Template
You create a notification report template to get a notification report when an alarm or a variable triggers a notification.
3/22/2017
Trend Chart Event Icons
Use the Trend Chart event icons to get information on different trend log events.
3/22/2017
​Configuring Server Port Settings
You configure server HTTP, HTTPS, and TCP ports to define the communication of the different protocols. In Software Administrator, you can configure either the ports of the Enterprise Server.
3/22/2017
Repairing the Enterprise Server
​​You repair the Enterprise Server installation if any problems are caused by the current installation.
3/22/2017

Product version

Language