Enterprise Server

944 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Adding and Removing Columns
You temporarily add or remove columns in a pane or View to get a better overview of the properties.
1/18/2018
User Account Group – Group Membership Tab
Use the Group Membership tab to edit the group membership settings of a user account group.
1/17/2018
Alarm Triggered Notification Properties - Basic Tab
Use the Basic tab to view or edit the properties of the alarm triggered notification.
1/11/2018
Variable Triggered Notification Properties - Basic Tab
Use the Basic tab to view or edit the properties of the variable triggered notification.
1/11/2018
User Account Properties
Use the User Account properties dialog box to configure the properties of a user account.
12/29/2017
Windows Active Directory User Groups
You can map Windows Active Directory groups to Building Operation user account groups if Building Operation runs on a network that uses this directory to manage users and user account groups. A Building Operation user account group that includes a Windows account group can be member of another Building Operation user account group.
12/13/2017
Creating a User Account Group
You create a user account group to make it easier to manage users who require the same software permissions and workspaces.
12/12/2017
DCU Device Properties – Message Distribution Tab
Use the Message Distribution tab to view and configure message distribution settings and reliable tap settings on the selected I/NET DCU.
12/5/2017
Alarm State Sort Order Dialog Box
Use the Alarm State Sort Order dialog box to change the order in which alarms of different states are displayed in the Alarms pane or the Alarm Views in the Building Operation system.
11/16/2017
Create Alarm Wizard – Attachment Page
Use the Attachment page to add attachments to an alarm or an alarm decoration.
11/6/2017

Product version

Language