Schedules

148 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Function Overview
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.
6/27/2018
5/21/2018
5/21/2018
Snap To Menu
Use the Snap To menu to select the time increments to display in the Advanced Schedule Editor when dragging a time value bar from the start to end time. The default time increment is 15 minutes.
5/18/2018
Storing Expired Calendar Events
You store expired events to keep an expired calendar event for future reference.
5/18/2018
Time Zones
When you create a schedule, the time zone of the EcoStruxure BMS server that contains the schedule determines the execution of the events. If the schedule is copied to an EcoStruxure BMS server in a different time zone, the specified dates and times relate to the new time zone.
5/18/2018
Viewing a Schedule Event
You view schedule events to see the schedule for one or more events.
5/18/2018
Viewing a Schedule
You view a schedule to add, remove, or edit events.
5/18/2018
Weekly Events in WebStation
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
5/18/2018
Weekly Events in WorkStation
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
5/18/2018

Product version

Language