Basic Functionality

530 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Products
Depending on your needs, you can install all Building Operation products or a few products, such a single SmartStruxure server device with a connected WorkStation.
3/29/2017
Object Properties
Every object in Building Operation has a number of different properties. Properties can be of two different types: read only and read/write. Read only properties are dimmed and cannot be changed. Read/write properties can be changed.
3/25/2017
Mass Rename
In WorkStation, you can mass rename all objects that are possible to move. For example, you can rename alarms but not properties.
3/24/2017
Server Installation Wizard – Configuration Page
Use the Configuration page to configure the port number the Enterprise Server listens to when communicating through a specific protocol.
3/22/2017
Repairing the Enterprise Server
​​You repair the Enterprise Server installation if any problems are caused by the current installation.
3/22/2017
WebStation Overview
WebStation is your web-based interface to your Building Operation system. You use WebStation to perform work on a daily basis in Building Operation.
3/10/2017
WebStation and WorkStation Differences
There are a number of differences in functionality between WebStation and WorkStation.
3/10/2017
Events Pane and Event View Toolbar
Use the Events pane and Event View toolbar to manage the events.
3/7/2017
Viewing Events in This Branch
You view events in this branch when you want to view all the events below a certain branch in the system. A branch can be any object that can contain other objects, for example, a folder or a network.
3/6/2017
Deleting a Favorite
You delete a favorite that it is no longer needed.
3/2/2017

Product version

Language