Alarms

318 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Creating a Notification Report Template
You create a notification report template to get a notification report when an alarm or a variable triggers a notification.
3/22/2017
How Alarms Work
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
3/15/2017
Alarm and Event Details
To quickly get all the details of a specific alarm or event in WorkStation, or an alarm in WebStation, you can use a Detail view. The Detail view always displays all properties that can be added and displayed in the Alarms pane, Events pane, Alarm View or Event View.
3/15/2017
Alarm Assignments
A triggered alarm can be manually or automatically assigned to a specific user or user group that seems to be most suited to correct the problem.
3/7/2017
Alarms Pane and Alarm View Toolbar
Use the Alarms pane and Alarm View toolbar to manage the alarms.
3/7/2017
Deleting a Favorite
You delete a favorite that it is no longer needed.
3/2/2017
Object-Specific Event View
Use the Object-Specific Event View to view events related to a specific object.
3/1/2017
Create Report Data Wizard - Configure Events Page
Use the Configure Events page to configure the content and the presentation of data in a notification report template.
1/16/2017
1/13/2017
Notification Reports
You can configure notification reports to include important information on the Building Operation system. Notification reports are distributed when a notification is triggered.
1/12/2017

Product version

Language