Alarms

319 Topic(s)
Use the filters below to limit the number of search hits.
Products
Information Type
Topic
Modified
Rating
Edit Checklist Dialog Box
Use the Edit Checklist dialog box to add, edit, or order the steps of a checklist.
10/12/2017
Edit Checklist Step Dialog Box
Use the Edit Checklist Step dialog box to edit a checklist step.
10/12/2017
Edit Favorite Dialog Box
Use the Edit Favorite dialog box to rename a favorite.
10/12/2017
Enumeration Alarm Properties – Basic Tab
Use the Basic tab to view or edit the basic properties of an enumeration alarm.
10/12/2017
Enumeration Alarms
​An enumeration is a variable with labeled values; different variables have different enumerations. When configuring an enumeration alarm, you configure the variable and its enumerations to monitor.
10/12/2017
Events Substitution Codes
Events substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the events that are included in the notification report.
10/12/2017
Extended Acknowledgement
When you select the acknowledgement type Extended acknowledgment, the user needs to acknowledge the alarm in the alarm view in reset state, before the alarm returns to normal state and disappears from the alarm view.
10/12/2017
Fault Style Properties
Use the Fault Style properties to edit and view the colors and fonts of alarms in the Alarms pane and Alarm Views that are in Fault state.
10/12/2017
Favorites Menu
Use the Favorites menu to apply, add, or manage Alarms pane, Events pane, Alarm View, Event View layout and filter conditions, or List View layout.
10/12/2017
Filter Condition Wildcards
A wildcard is one or more characters used to simplify the process of setting up filter conditons. You use wildcards to substitute characters or combinations of characters in object properties, such as names or descriptions. For example, instead of setting up five filter conditions for values with names beginning with a, b, c, d, or e, you can set up one single filter condition for values with a name beginning with any of the characters in the range [a-e].
10/12/2017

Product version

Language